AXIS#.SAFEPARAM.SDI.FUNCTIONACTIVATION

Description

Indicates whether the Safe Direction (SDI) safety functions can be activated. This applies for both SDIp (positive) and SDIn (negative). One of the following values can be used:

Value Description

0

Never active

1

Ready for activation

This function can only be used when a safe encoder is configured in the safety parameters.

 

Parameters Editor with all values for Function Activation shown and circled

Context

For complete SDI information refer to SDI (Safe Direction)

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0 (Never active)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SDI.FUNCTIONACTIVATION

3164h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SDI.FUNCTIONACTIVATION

3264h

01h

Unsigned8

-

-

Read/Write

No